This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

802.15.4 multipoint to point link using CC2630/40/50

Other Parts Discussed in Thread: CC2630, TIMAC, CC2650, CC2540, CC2500

Hi,

Are there any plans to produce / release some sample code which would allow a multi-point to point link based on 802.15.4 (not BLE or Zigbee), a basic TX to RX example using CSMACA and CC2630's, 40's or 50's?

I read somewhere that the basic packet test code running on the CC2650 Development Kit will not be made available due to licensing restrictions and that TIMAC is limited to 100kbps throughput (we would require at least 1Mbps).

I have looked at the Temperature Sensor Node but this uses BLE and a CC2540 as the receiver.

Thanks.

Active