Other Parts Discussed in Thread: CC2541, CC2640
Hello,
I want to use the GattNotification commande like :
GATT_Notification(0, ¬i, FALSE);
but i have an error : No source available for "xdc_runtime_Timestamp_get32__E__mangled__() at ....
I want to precise i worked on a CC2541 before, with the BleBridge project. My cc2541 project worked fine, and now i work on cc2640 and i try to translate the code to send a notification over UART.
I think GattNotification can only used in Stack Project.
I want to use GattNotification in my Application Project. How ?
This is my code :
case ID_COMMANDE_NOTIFY:
len_notification = pCmdMsg->pData[2];
len_notification = 2;
uint8_t packets_sent = 0;
//on s'assure que la file d'attente de la notification est réussie
bool send_error = FALSE;
//la valeur de retour pour mettre à jour la queue et envoyer ack
uint8_t bytes_sent = 0;
attHandleValueNoti_t noti;
//dummy handle
noti.handle = 0x59;
//counter
uint8_t i = 0;
while ((packets_sent < 4) && (len_notification >= 20) && (send_error == FALSE)) {
value = &rxdata[0];
//send 20 bytes
noti.len = 20;
for (i = 0; i < 20; i++) {
noti.pValue[i] = rxdata[bytes_sent + i];
}
//connection handle hardcoded
if (!(GATT_Notification(0, ¬i, FALSE))) //if sucessful
{
bytes_sent += 20;
len_notification -= 20;
packets_sent++;
} else {
send_error = TRUE;
}
}
//last packet
if ((packets_sent < 4) && (len_notification > 0)
&& (send_error == FALSE)) {
noti.len = len_notification;
for (i = 0; i < len_notification; i++) {
noti.pValue[i] = rxdata[bytes_sent + i];
}
if (!(GATT_Notification(0, ¬i, FALSE))) //if sucessful
{
bytes_sent += i;
len_notification -= i; //number of byte send
} else {
send_error = TRUE;
}
}
break;
Thank you.
Best regards,
Steeve