hi,
i use the CC256X Bluetooth Hradware Evaluation tool to do the BT test.
my HW connection:
PC ( With CC256X Bluetooth Hradware Evaluation tool )<- USB-Serial Bridge -> CC2564MOD. Baud rate: 115200
the SP version is 1.2
every time i power up the system, download the SP to CC2564MOD, then send the HCI UART TX(PC to module) command, but there's no response till message "Com port time out".
i can sure that the slow clock and SHDN have normal input to CC2564MOD, and i try to swap the TX & RX pin, but still happen "Com port time out"
i need a hint how to solve this problem, thank you.