This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 ModbusPeripheral Advertise Continuously

I built the Modbus 485 board and I am using the ModbusPeripheral program to connect to some equipment. The board is wired to a DC power source so I am not worried about power consumption. Also using a button to advertise won't be feasible. I need to advertise continuously whenever not connected to a phone.

I've been messing with the preprocessor definitions, timing settings and I put GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8), &advertising); in the GAPROLE_WAITING case in ModbusPeripheral.c, but every adjustment I make I think it is making it worse.

Thank you in advance.

  • Hello Eric,

    You want to make sure your Adv flags are defined as follows:

    #define DEFAULT_DISCOVERABLE_MODE             GAP_ADTYPE_FLAGS_GENERAL

    to enable continuous Advertising.

    Best wishes