We noticed that it's claimed in CC2564MODN's datasheet that:
Fully Certified Bluetooth 4.1 Module
– Compliant Up to the HCI Layer
– FCC (Z64-2564N)/IC (451I-2564N) Modular
Grant with External Chip Antenna (see
Section 6.2.1.3, Antenna)
– CE Certified as Summarized in the Declaration
of Conformity
– Bluetooth 4.1 Controller Subsystem Qualified
(QDID 55257)
Does this mean if we use CC2564MODN on our board, we can use it's FCC and CE certification directly and don't have to do these cetifications by ourselves?