I have a simple question (hopefully) regarding the BLE stack's spacing of peripherals. From what I've observed with a scope, whether the connection interval is 100 millisec or 10 millisec, two peripherals connected to the central seem to have their connection windows setup with a 5 millisecond spacing from eachother. Is this constant for all connection intervals and scenarios or is there some cases where this may change?
On a related note, does this mean the max peripherals under the minimum 7.5 millisecond connection interval is two?
Thanks!