This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLE Stack V2.1 - Reading connection interval from central role?



I understand that for peripheral roles, there is the GAPRole_GetParameter function which would allow one to obtain the connection interval that it is currently running at. Is it not possible to obtain this value on the central side? E.g. if two peripherals are connected and I wanted to know the connection intervals for both of them? Is the only way to to do the commands on the peripherals and transmit the values back to the central?