Hello,
I'm developing some ble applications on the CC2541 using IAR. I am using the HM10 module for the purpose. Can someone point out the exact version of iar on which the sample projects provided with the stack was created? The created hex file generated on compilation and those provided along with the stack seem to vary. The present problem is that the peripherals seem to work fine, but no BLE packets are being broadcast. It would be very helpful if someone provided a hex file that has been tested on hm10 so that i can confirm that it is not any kind of hardware or antenna issue.
Thanks