This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODN module dimension error

Other Parts Discussed in Thread: CC2564MODN

The current CC2564MODN spec (SWRS160B REVISED JULY 2014) appears to have a dimensional error on page 39. We would like to know what the correct dimensions are. I have created a PDF file which contains a graphic which clearly shows the error, which I have attempted to attach. To explain as best I can without the graphic, the width of the module is 7.0 mm. Using coordinate x = 0 as the center, coordinate x = -3.5 is obtained by adding:

0 - a1/2 - c3 - a1 - b3 = -3.5 mm

However, adding the pad widths and gaps across the bottom produces x = +3.4 at lower right corner. It should be x = +3.5.

How soon can we find out the correct dimensions for the CC2564MODN pad locations?CC2564MODN_IC_Mechanical.pdf?