Dear TI engineer,
I have a question now.When I use pwm driver ,I call the function of pwm driver ,but the project can not pass compile.Blow are my code and errors.I have seen the use guide .I don't know what does this "
To enable this driver, add the following statement to your application’s *.cfg file.
TIRTOS.usePWM = true;"  mean .
When I put this code in appBLE.cfg(I use sensor tag application ). The project can not pass compile. Thank you.
"
MY CODE
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/family/arm/cc26xx/Power.h>
#include "type.h"
#include <ti/drivers/i2c/I2CCC26XX.h>
#include <driverlib/prcm.h>
#include <ti/drivers/PWM.h>
#include "Board.h"
#include "sensor.h"
//#include "bsp_pwm.h"
PWM_Handle handle;
PWM_Params params;
uint8_t pwmOutputNumber = 0;
extern void PWM_Params_init(PWM_Params *params);
//au();
PWM_Params_init(¶ms);
ERRORS
Error[Pe079]: expected a type specifier
Error[Pe260]: explicit type is missing ("int" assumed)
Error[Pe147]: declaration is incompatible with "__interwork __softfp void PWM_Params_init(PWM_Params *)" (declared at line 467 of "C:\ti\tirtos_simplelink_2_13_00_06\ C:\ti\simplelink\ble_cc26xx_2_01_00_44423\Projects\ble\SensorTag\CC26xx\Source\Application\Board_patch\Interfaces\bsp_pwm.c 65