Other Parts Discussed in Thread: CC2592, CC2650
Hi,
I am using CC2650_5XD board interfaced with CC2592 RF Front End.
I had modified "SimpleBLEPeripheral" project in CCS as below:
1. In Project Properties,changed the Include Options from "${TI_RTOS_DRIVERS_BASE}/ti/boards/SRF06EB/CC2650EM_7ID" to "${TI_RTOS_DRIVERS_BASE}/ti/boards/SRF06EB/CC2650EM_5XD"
2. Removed "TI_DRIVERS_LCD_INCLUDED" from predefined symbols.
3. In main.c file of Application Project:
[In our PCB, CC2592_PA_EN is connected to DIO_7 , CC2592_LNA_EN to DIO_8 , CC2592_HGM to DIO_9]
int main()
{
PIN_init(BoardGpioInitTable);
CC2592_io_init(); //For Configuring CC2592
/* Initialize ICall module */
ICall_init();
/* Start tasks of external images - Priority 5 */
ICall_createRemoteTasks();
/* Kick off profile - Priority 3 */
GAPRole_createTask();
SimpleBLEPeripheral_createTask();
/* enable interrupts and start SYS/BIOS */
BIOS_start();
return 0;
}
4.In SimpleBLEPeripheral.c:
static void SimpleBLEPeripheral_init(void)
{
ICall_registerApp(&selfEntity, &sem);
HCI_EXT_SetTxPowerCmd(HCI_EXT_TX_POWER_5_DBM);
// Create an RTOS queue for message from profile to be sent to app.
appMsgQueue = Util_constructQueue(&appMsg);
--------------------------
// remaining code as it is
--------------------------
}
But, the problem I am facing is I am trying to connect the peripheral but within 10sec due to "Connection Timeout" , peripheral is getting disconnected(even though while reading the UUIDs, in the mean time it is getting disconnected). I am able to connect the peripheral within 10meters range only.Can anyone help me to solve this.
Thanks.
Regards,
Anuhya.