Other Parts Discussed in Thread: CC2640
Hi folks,
I have did a few test related to multi connections and multi roles firmware. I suppose to develop a multi role firmware which can support up to 6 or more connections. However, according to my test and this post e2e.ti.com/.../1547124 , the sample project of multi-role can only support 4-5 connections. It seems that the size of SRAM is the main limitation.(because the 20k SRAM was almost fully occupied when I configured the HEAPSIZE to 8000) I wonder if it is possible to extend SRAM size so that it can support more stable connections? Or if there is other powerful microchip from TI or other provider can support more simultaneous connections as well as the multi-role function?
Cheers,
Kai