Other Parts Discussed in Thread: CC2640, CC2564
Hello
i'm starting a proyect where i need to include a Bluetooth connection (1st time for me).
The device is battery powered and has to last some years with a single battery.
I found the CC2640 which seems to be a adequate BLE chip for me.
The bluetooth connection will be used at max only 1 time per month. Someone with a mobile phone (Andoid) will
connect to my device and read out the datalog. The device will have no buttons or wired connections to turn bluetooth on.
So, my question is about the power usage of the CC2640 when he is discoverable.
I think the device should make itself discoverable 1 or 2 times per minute, am i right?
In the datasheet http://www.ti.com/lit/ds/symlink/cc2640.pdf (at page 28) are the power modes.
Is the device in "idle" mode (550 µA) discoverable? How long is the recomendation to stay discoverable?
Are there some guidelines/recommendations about this topic?
For me the 550µA during discoverable mode seems to be high, because the CC2564 http://www.ti.com/lit/ds/symlink/cc2564.pdf
I hope you can help me with his, i read a lot in diferent forums and web pages (of course http://processors.wiki.ti.com/index.php/Category:BluetoothLE?DCMP=blestack&HQS=ble-wiki )
but couldnt get a clear answer.
Best regards,
Dorian