This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash error

Other Parts Discussed in Thread: CC2650

Hello,

I am facing problem when trying to flashing my binary..the following error getting every time and I have tried with flash programmer tool over there i was trying with option mass storage erase  in settings but still i am facing issue.

11:58:23 **** Build of configuration Default for project TDL ****
mingw32-make.exe makefile=makefile BCDS_DEVICE_ID=CC2650EM_7ID flash_d
Running On MINGW32_NT-6.1;  USING  IAR version V7.40.2.8542/W32
working on target dev_id
XDS_DEVICE_ID=['XDS-06EB1221290EA']

"C:/Program Files (x86)/Texas Instruments/SmartRF Tools/Flash Programmer 2/bin/srfprog.exe" -t "soc(, CC2650)" -e all -p "epfw(0)" -v rb -f "D:/TDL_PROJECT_DEV/tdl/TDLApp/resources/stack/iar/SimpleBlePeripheralIarStack.hex" -a 0x0000D000

Texas Instruments SmartRF Flash Programmer 2 v1.6.3-windows
-------------------------------------------------------------------------------

Reading file: D:/TDL_PROJECT_DEV/tdl/TDLApp/resources/stack/iar/SimpleBlePeripheralIarStack.hex.
Start flash erase ...


Flash loader reported an error (4)
Reset target ...

OK
"C:/Program Files (x86)/Texas Instruments/SmartRF Tools/Flash Programmer 2/bin/srfprog.exe" -t "soc(, CC2650)" -p "epfw(0)" -v rb -f D:/TDL_PROJECT_DEV/tdl/TDLApp/debug/.hex -a 0x0

Texas Instruments SmartRF Flash Programmer 2 v1.6.3-windows
-------------------------------------------------------------------------------

Reading file: D:/TDL_PROJECT_DEV/tdl/TDLApp/debug/.hex.
Start flash programming ...

0%

0%
Flash loader reported an error (4)

Reset target ...

OK
Error occured at addr: 0x00000000, writing 16768 bytes.