Other Parts Discussed in Thread: CC2560
Hi,
oes the GAPRole_TerminateConnection function of the CC2560 BLE-STACK-2-1 terminate the connection by using the MD bit in the link layer or does it force a disconnection?
Many thanks and best regards
Marcus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2560
Hi,
oes the GAPRole_TerminateConnection function of the CC2560 BLE-STACK-2-1 terminate the connection by using the MD bit in the link layer or does it force a disconnection?
Many thanks and best regards
Marcus
Hi Eirik,
many thanks.
Do we have a way in the BLE-STACK-2-1 to terminate a connection by using the MD bit?
Many thanks and best regards
Marcus
Hi Eirik,
is my understanding correct.
We do not really support the MD bit. this may lead to the matter of the fact that TI Stack may terminate the link while the remote device still wants to send something.
The solution to this is try to handle this in the application layer?
Many thanks and best regards
Marcus
Hello Marcus,
No:
The TI stack has implemented the Bluetooth core specification and the link layer support the :
If either or both of the devices have set the MD bit, the master may continue the connection event by sending another packet, and the slave should listen after sending its packet. If a packet is not received from the slave by the master, the master will close the connection event. If a packet is not received from the master by the slave, the slave will close the connection event. This means that the slave should listen if the MD bit is set, but it does not have to and can close the connection and terminate the connection before the additional data is received.
"4.5.6 Closing Connection Events" in Bluetooth® Core Specification.
and Yes:
Depending on what you do, you need to handle this in the application. If for example you have queued notifications you must simply wait until the next connection event before more notifications is sent to the peer device.