I am working on a project that requires a continuous connection 24/7 between a peripheral device using CC2640 and iOS. There isn't a lot of data exchange between the two devices, but I have to maintain the connection to improve system responsiveness.
1. What are the connection parameters on the CC2640 to achieve this continuous connection?
2. What is the power consumption on CC2640 to do so?
3. Will continuous advertising in 2 sec interval achieve the same effect?
Thanks,
Bryan