This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564 MODN BT Stack VS_Set_Max_Output_Power issue

Other Parts Discussed in Thread: CC2564

Hello there. 

Do any known issues or errata exist for the VS_Set_Max_Output_Power command in the latest Bluetopia stack on MSP430?

Just after initialization I change it to 12 (highest power?) and am getting reasonable range.  But in testing it I am finding no difference in current consumption or apparent range from 0 to 12.  Perhaps this command can only be issued at certain times?  ie.  not while an SCO connection is active.  Result code returned is 0 in all cases. 

I had read that the transmit power is actually hard-set in the CC2564.  Though others claim that isn't the case.  Couple of confusing threads on here about it.

Any help would be appreciated!

 - Jason Gossiaux