This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: Toggle the Protocol by pushing the user button

Guru 24520 points

Other Parts Discussed in Thread: CC2650STK

Hi community member,

Please let me confirm the following questions.
[Question]
According to the introduction page, it seems that the CC2650STK can toggle the protocol by pushing the user button.
Does this function implement on the current firmware?

 

If you have any questions, please let me know.
Best regards.
Kaka

  • Hi Kaka,

    Yes, it is possible on the Sensor tag V2.0 to toggle protocols, can you specify which firmware you are using?

    Thanks,
  • Hi,

    Thank you for your response.
    I use the V1.12 firmware for sensortag.
    Have you already released that firmware which it can toggle protocols?
    I checked the senortag app on iOS, I could not find this.

    Best regards.
    Kaka
  • Hi you should find it here:
    C:\Program Files (x86)\Texas Instruments\SmartRF Tools\BLE Device Monitor\firmware\cc26xx

    after installing the latest version of BLE Device Monitor.

    Best wishes
  • Hi
    I have already installed the BLE monitor. And find the firmware for CC2650STK.
    Which firmware support the multi protocol?
    I found the following latest firmwares.
    - CC2650SensorTag_BLE_All_v1_20.hex
    - CC2650SensorTag_BLE_App_v1_20.hex

    Best regards.
    Kaka
  • Hi,
    It should work as follows:
    First upgrade to the latest BLE image (BLE_All).
    In order to switch from BLE to ZigBee, the ZigBee-image is downloaded as a normal OAD, and the after OAD has completed it reboots using this new image.
    To switch back to BLE the user needs to press both buttons for 6 seconds and the factory programmed BLE image will be loaded from external flash and the device rebooted as BLE.
  • Hi,

    Thank you for your response and kindly detailed explanation.
    I checked this and it works well.
    But the Sensor tag introduction page said that CC2650STK can toggle some protocols(BLE/Zigbee/6LowPAN) with hold the user button three seconds.
    Do you also provide this firmware?

    Best regards.
    Kaka