Other Parts Discussed in Thread: CC2650STK, CC2650
Hi everyone,
I apologize for the question, I am new to this and I am sure it is pretty trivial.
I am designing and building a precision agriculture system for a senior project using two CC2650STK+CC-DEVPACK+Grove modules as the nodes. Due to the location, I will need to setup a coordinator that will be able to pull data from these nodes, send it to a computer nearby and with a response from Sensor Controller Studio, activate solenoid drivers to allow automated irrigation. I am communicating via BLE.
My question regards what would be best suited for the coordinator. It seems like a CC2650DK would be excessive and I was wondering if I would be able to just use a single SmartRF06 evaluation board with the CC2650 Evaluation module kit. Would the evaluation module kit also be suitable for communication from the two nodes to the board and from the board to the solenoid drivers? Would I then have to communicate to a computer with a Bluetooth dongle?
Like I mentioned before, I am sure this is pretty simple but something that I haven't been able to find a suitable answer on.
Thanks,
Justin P.