Other Parts Discussed in Thread: CC2640, BLE-STACK
Hello,
I have a strange phenomenon with the CC2640 on a custom board that I made and I was wondering if you might have any tips to find out the source of this behavior.
I took the standard sensor tag program (first stack and then application) and loaded it to the device via the debugger. I hit run in debug mode and I can detect my custom board via the sensor tag app on my android phone. However, when I turn off the power to the board and disconnect the debugger from the board and then turn the power back on the program doesn't run on the CC2640. I know that since the board is not longer detectable on the sensor tag android app.
Then, I took the sensor tag application project on CCS6.1 and modified it by adding a task that constantly blinks an LED on my custom board. It works great via the debugger. But after I disconnected the debugger and reset the board power the software just doesn't run on the CC2640 since the LED doens't blink.
Another thing that I noticed is that if I click on the "Terminate" button in CCS6.1 during debug mode then the debugger stops (of course) but then the application on the CC2640 continues to run (or resets - I don't know for sure). At that point I can disconnect the debugger cable from my board and the application is still running. But then when I turn off the power and turn it back on the application does not run anymore.
I must add that I soldered the CC2640 IC to the board myself using a hot air blower. Could I have damaged perhaps the chip? At first that is what I had thought so I removed the chip, and put a new one using the same soldering method and I still see the SAME behavior. I don't understand why the program doesn't run on the IC when I reset the power.
I don't get it. I have a SensorTag and I checked and saw that unlike my custom board, if I take out the coin battery and put it back in then it simply resets and does works again (without any connection to my debugger).
Any thoughts?
Thanks,
Eyal