This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DEVPACK-WATCH and CC-DEVPACK-DEBUG

Hi,

I'm using sensortag with display DEVPACK-WATCH and it works fine when it is connected directly on sensorTag but it is rather annoying to unplug debugger, connect display and test firmware each time I modify something. Is there a way to work with display connected to the second LSS-110 connector on the other side of debugger?

I've take a look at the schematics, the 'second' connector is an exact copy of the sensorTag side LSS-110 connector (only pins 17 and 19 are different, but I don't think they are used by the display), so, why doesn't it work?

Davide.