Other Parts Discussed in Thread: CC2640
The ADC description in CC2640 TRM (rev d) on page 1212 states that with scaling disabled the reference is 1.47V. And with scaling it looks like 4.3V even though in recommended max is 3.8V?? (I heard the 4.3V caused flash failures). However, in the data sheet (Oct 2015) it states the reference is 1.44+-1% (1.45V max). When I input an exact voltage, without scaling, of 1.470V the ADC outputs 4095. I tried this on several modules with the same result, +- 1 LSB. It looks like the TRM is correct and the data sheet is incorrect. This is an important specification and I can't trust it yet. Does anyone know the true value?