Other Parts Discussed in Thread: CC2541, CC2640
we have a project, with power saving, running on a board, everything is ok, current is 0.5mA at bluetooth advertising, and 1uA when sleep.
but, exactly the same project, run on another board, which is more simple, no IO is connected, but current is strange 7-10mA at first, then go to sleep 1uA.
we have tried all IO setting, including set it IO, input with pull up/pull down, or 3-state, or out, nothing help.
our project has no iic or uart work.
why? should not be board problem as we tested several (at least five) boards
help!