I am trying to connect one of the SPI modules in the CC2650 chip to the following pins:
SCLK: DIO_10
CS: DIO_11
MOSI: DIO_13
MISO: DIO_20
We are not using the MISO functionality, but I have connected it to DIO_20 (which is unconnected on our custom board).
When I call the RTOS function SPI_open, which I expect to return a handle to an SPI “object”, it returns null.
If I modify the pins I am trying to connect the SPI peripheral like so:
SCLK: DIO_18
CS: DIO_15
MOSI: DIO_6
MISO: DIO_1
The SPI_open function returns a valid handle.
When I try making a call to SPI_transfer with the null handle while running in debug mode, I can see that the program calls the loader_exit function in the file exit.c.
When I make the call to SPI_transfer with the valid SPI handle, the chip behaves as expected. The SPI_Transaction object is the same in both test cases.
All of the pins in question (the set that work and the set that don’t) are accessible on the smartrf board. I have tried running the code both on our custom board and one of the development boards and the debugger behaves the same in both cases.
The set of pins that work are labeled as follows on the smartrf board:
SCLK: RF1.8
CS: RF1.6
MOSI: RF1.4
MISO: RF1.5
The set of pins that does not work are labeled:
SCLK: RF1.16
CS: RF1.14
MOSI: RF1.15
MISO: RF2.8
Has anyone successfully used the RTOS function SPI_transfer function that could help me overcome this NULL issue?
Thanks!