This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to receive notification in multi2.1 project?

Hi all.

I use multi 2.1 project. When connection is done with slave, slave starts to send notification with 1000ms interval .

I used folow code for receiving notification in old multi(2.0) project:

static void SimpleBLEMulti_processGATTMsg(gattMsgEvent_t *pMsg)
{
if ((gapRoleNumLinks(GAPROLE_ACTIVE_LINKS) > 0))
{

if (pMsg->method == ATT_HANDLE_VALUE_NOTI ||
pMsg->method == ATT_HANDLE_VALUE_IND)
{
attHandleValueNoti_t noti;

noti.handle = pMsg->msg.handleValueNoti.handle;
noti.len = pMsg->msg.handleValueNoti.len;
noti.pValue = pMsg->msg.handleValueNoti.pValue;

TLwrite(noti.pValue, noti.len);

.........

in multi 2.1 it doesn't work. In debugging I see that Process GATT messages and events not happen.

I see notification messages in packet sniffer.

How to receive notification messages in multi(stack 2.1) ?

Thanks