Other Parts Discussed in Thread: CC2640, CC2650
Hi,
We are building custom board of CC2640 and faced some issue in programming and solved by help via this e2e thread.
https://e2e.ti.com/support/wireless_connectivity/f/155/t/466047
Now, we are testing throughput with android mobile by verifying the timing with snoop logs. we need to achieve more than 16K Bytes per second.
Right now we are able to achieve 12k with connection interval 20ms with MTU changed to 255 with nexus 4(android - 5.0 & Bluetooth version 4.0 ).
If we reduce the connection interval to 15 , with snoop logs data are getting corrupted.
we are looking for information on the maximum number of packets which we can transmit in one connection event.
Kindly help.