Hi, i've a problem with my beacons.
I've a beacon set to function as Advertiser and your period adv is set to 100ms, another beacon is set to function as Observer and your obs scan period is 200ms.
The system works until beacon distance are less 6-7 meters, but when I increase the distance between beacons, i can't read the rssi of the beacon in adv?
There is a setting, for observer beacon, that can i used to permit reading of rssi very low?
thanks