This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 ANCS Sample

Other Parts Discussed in Thread: CC2640, CC2650

The CC2640 ANCS sample as below link :

processors.wiki.ti.com/.../Cc2640_ANCS_Sample

I used the CC2640 ANCS sample to test  ANCS function, and my BLE target board is CC2650 daughter board + RF06, when my target board successfully doing the BLE pairing with my iPhone(ios8.x), it shows the pairing successful message with which cell phone I paired on the LCD of RF06.

But if the ios is 9.1, it shows nothing on the LCD, and also the caller ID and message can not showed on the LCD if the ios is 9.1. Why is that?