I'm using the SimpleBLEPeripheral and SimpleBLECentral projects (CC2640 chips) to implement notification sending. I'm trying to send 1 notif every 100 ms, but on the Central side, it looks like I'm actually getting a burst of 10 notifs once every second. I feel like either there's a parameter on the Peripheral that queues notifs and sends them once a second, or one on the Central that calls processGATTMsg once a second to handle all built-up messages. Is either guess accurate? Thanks!