Other Parts Discussed in Thread: CC2540
Hi all,
I implement the multiple slaves to connect to one master for BLE. Before the connection, I have already set the connection interval individually for each slave, and when I connect to master, all connection interval is set to 100ms. And I could only adjust the interval as 50ms and 100ms, the other interval could not be assigned ex,. 70ms or 120ms.
Could any one help me what happen in this case and with this problem means the slave's connection interval could not set by itself?
(I implement this experiment with CC2540)
Thanks