Other Parts Discussed in Thread: CC2540, CC2541
Hi,
Thanks to your continuous support, we are close to production phase of our first hardware project.
I was investigating OAD and found out that it is possible to program Image B without the OAD support. (Since the configuration is available at buildConfig.cfg).
However, when I tried loading image B without OAD support using BLE device monitor software, it does not detect the user ID or the program as a valid one. If I use FEATURE_OAD, then image B will be detected in Device monitor and everything goes smoothly.
I have only CC Debugger and CC2540 USB Dongle with me so the actual solution given in the wiki for programming is of little use. I just want to know whether this is a limitation of Device monitor software or the hardware.
Using CC2541 with BLE stack 1.4.1.