Other Parts Discussed in Thread: CC2650
I am facing an issue with the CC2650 in Central mode. Once the connection is established, sometimes the device disconnects from the peripheral. I could see the disconnect event on the peripheral but CC2650 doesn't enters the GAP_LINK_TERMINATED_EVENT . 2650 still assumes its in connected state. Is there a way to determine the connection status or a way to determine if I am still connected to the peripheral (considering 2650 never enters the disconnect)