Other Parts Discussed in Thread: CC2650, CC2590
Hi
We are facing strange problem with custom board based on CC2650.
When we connect JTAG emulator XDS200 with CC2650, the program executes and works as expected (like we are able to toggle GPIOs, communicate using UART etc...)
We are also able to successfully write flash using debug interface.
After flashing we power cycle the board but then nothing happens after that. It looks program doesn't start executing.
We have tested 10 boards out of that 5 boards having such issue, other 5 boards are working fine after power cycle.
For troubleshooting we have verified below thing:
1. Tried to read back the flash again and verified that content written same as expected.
2. Verified reset circuit & its relation with VCC.
3. Different the crystal parts if there is clocking problem
but none of the trial worked.
Can anybody help me to explain possible problems that causes this strange behaviour?
Regards,
Bipin