This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Immediate Alert profile is not Working when i have updated firmware to stack 1.4.1

Other Parts Discussed in Thread: CC2541

Hi All,

Can anybody suggest me for this issue,

I have updated my firmware from the old stack 1.3.2 to stack 1.4.1 and my immediate profile is not working in the firmware,

is there any specific changes i need to done in the firmware which i may have missed any suggestions 

Best Regards

 Atul

  • How are you testing it?
  • I am testing with the third party app BLE utility when i am sending any code the device is not receiving it but it is connecting and disconnecting properly.

    also i debugged putting breakpoint in firmware where it receives the immediate alert code it is never entering that loop.

  • Hi Tim,

    Any Suggestions ..?

    I am using Keyfob code and immediate alert  levels the one which are predefined in the default keyfob code are working fine,

    in the KeyfobApp_PerformAlert if i am defining some more alert levels those it is not receiving,i am also defining those alert levels  in the Proxreporter.h file

    on CC2541 i am testing it using cc debugger.

  • Hello Atul,

    For the added levels, did you also add the logic to the respective WriteAttrCB & SetParameter functions in proxreporter.c? I would trace the code flow using the CC Debugger from the callback all the way to your app. Just defining additional levels in proxreporter.h is not sufficient.

    Best wishes