I would like to use the CC2640 Sensor Controller to interface to two SPI peripherals. Each has its own MISO signal. This is necessary since the peripherals don't release (tri-state) their MISO signals when the SPI select is de-asserted.
I see how to "connect" the software-based Sensor Controller SPI to the appropriate pins via the GUI in the Sensor Controller Studio. But this forces me to select a single pin for the MISO function.
Is there a way to connect the MISO signal programmatically so I can "switch" the MISO signal pin at the appropriate times?
I don't see an API call to do this...
Thanks!