Other Parts Discussed in Thread: CC2650
Hi,
Is there any sample project to read temperature using integrated sensor in CC2650? Thermometer example is using button press as temparature input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2650
Hi,
Is there any sample project to read temperature using integrated sensor in CC2650? Thermometer example is using button press as temparature input
ya, i tried that. but it still on 25. when i place it near a soldering iron , it rise upto 40. but my doubt is , why its hows 25, even if room temparature is 30?
andwhy i gets incorrect reading (10) when i change code like this
while(1)
{
AONBatMonEnable();
TemperatureSensor = AONBatMonTemperatureGetDegC();
printf("%d\n", TemperatureSensor);
AONBatMonDisable();
}
is this the correct way to turn off and on sensor?
The temperature sensor have +/-5c error. It's easier to test it if you have something other than 20~30 environment to see the difference
so if m sensor reading is 25 Deg C, actual reading may be between 30 and 20 right??. I have tested it near soldering iron and it rads as 40C