Other Parts Discussed in Thread: CC2650
Dear All,
I am using example project of OAD for ON Chip. It is taking 360ms for sending each packet. After changing the connection interval to 8ms Time for sending each packet is reduced to 100 - 110 ms. Still I want to decrease the time. I want to send each packet for minimum connection interval that is 8ms. Then what is the change I have to do in the OAD Image A i.e., OAD Transfer Image. Is any one already tried please help me on this.
For data transfer from Master side I am using BLE112 dongle.
Connection interval on both side (BLE Dongle and TI cc2650 side) Minimum & Maximum --> 6 & 7 (multiple of 1.25ms)
Thanks for your support in advance.
Thanks,
Siva.