Other Parts Discussed in Thread: CC2650
Hi
I have a cc2650 running on HostTestx connected to external MCU over uart.
I have been able to execute most of the GAP/GATT functionalities using the TI VS commands from the external MCU.
Now, the requirement is to do compliance tests, similar to the one that is done using SmartRF studio tool. We cannot use SmartRF tool since
the cc2650 is embedded into our custom board. I tried BTool on SmartRF06 EVB and played around with those HCI_Ext and HCI command related to the HCI_LEContinousTx , Rx but I don't see they are working like SmartRF06 does.
Is there any documentation available that explains this? What options I got to explore?
I presume HostTest firmware should work for these compliance tool, since SmartRF tool works.
Thanks
Damo