Other Parts Discussed in Thread: CC2650
Hey,
I am developing CC2650 with CCS, somewhere the application stops working (I have a periodic task that change the adv data every 20 ms, so using sniffer I see that it continue to transmit the same packet which means that the periodic task stopped working)!
then every time I make Pause I see it is in the Void Power_standbyPolicy() at CPUcpsie();!
if I try to restart and relaunch from the CCS it has no effect!
till I stop/terminate the program and then launch from the beginning!
what is the problem do you think and how can I solve/work around?!
Thanks.