Other Parts Discussed in Thread: CC2564MODAEM, CC2564
Can someone see something I have missed doing below in trying to setup a simple BT "headphone"?
Just bringing up the evaluation stack first time. The "SPPDemo" appeared to be working before trying the A3DPDemo_SNK sample.
We have the CC2564MODAEM attached to an STM32F4-Discovery board with the CC256XEM-STADAPT V1.0.
1. Android 4.0.4 shows BT pair with "A3DPDemo_SNK", Headphone symbol
2. Music file playing on Android was 44.1K, sound played on phone speaker, sound did not transfer to Discovery phono jack output and silence phone speaker as expected.
3. Zero ohm resistors R32, R12, R22 and R54 installed on CC256XEM-STADAPT.
4. Did NOT install CC256XEM-STADAPT "AP Connectors" since '407 pins already connected to CS43L22 I2C (PB9/PB6).
Console text copy:
OpenStack().
Bluetooth Stack ID: 1
Device Chipset: 4.1
BTPS Version : 4.0.2.1
Project Type : 6
FW Version : 7.26
App Name : A3DPDemo_SNK
App Version : 0.1
BD_ADDR: 0x0017E9E579AA
Mute and enter the DAC, CS43L22, into power save mode with reset
A3DP Endpoint opened successfully.
Class of Device: 0x040424.
Supported formats:
Frequency: 44100, Channels: 2, Flags: 0
Frequency: 48000, Channels: 2, Flags: 0
Frequency: 48000, Channels: 1, Flags: 0
Frequency: 44100, Channels: 1, Flags: 0
******************************************************************
* Command Options: Inquiry, DisplayInquiryList, Pair, *
* EndPairing, PINCodeResponse, PassKeyResponse, *
* UserConfirmationResponse, *
* SetDiscoverabilityMode, SetConnectabilityMode,*
* SetPairabilityMode, SetBaudRate *
* ChangeSimplePairingParameters, *
* GetLocalAddress, GetLocalName, SetLocalName, *
* GetClassOfDevice, SetClassOfDevice, *
* GetRemoteName, OpenSink, CloseSink, *
* RemotePlay, RemotePause, RemoteNext, *
* RemotePrev, Help *
******************************************************************
A3DP+SNK>OpenSink
Endpoint is already opened.
Function Error.
A3DP+SNK>
A3DP+SNK>RemotePlay
A3DP Stream is not opened yet.
Function Error.
A3DP+SNK>RemotePlay
A3DP Stream is not opened yet.
Function Error.
A3DP+SNK>