hiiii
i want to set the authentication for my bluetooth device while pairing
fallowing config are done -> mitm=true and pairing mode to initiate and remaining as mentioned in the user guide
i can able to set the pairing pin and from mobile i can enter the pin it is pairing
problem faced are:
1. i have given password as 123456 .and when i try to enter 12345678 from mobile it is pairing where as the password is just 123456 only which is 6 dig length
and when i enter passwords like 123456,12345678,123456789 it is pairing (passcode i set is 123456)
2. and onemore case is of entering password is not working if we fail to set password for 3 times after wards it is directly pairing
could you please suggest me whether i missed any changes from the embedded side or we have a limitation from bluetooth????
devices are devkit-cc2650 in simple ble peripheral mode mobile-nexus6
pls suggest!!!!
thanks in advance