Hello all,
Thank you for reading this post. I saw a lot of posts regarding connection between CC debugger and keyfob device.
I just received mini dev kit which contains cc debugger, cc 2541 keyfob model and usb dongle.
I installed cc debugger driver. The flash programmer detected my cc debugger and I was able to update to the latest revision.
I connected my cc 2541 keyfob but flash programmer cannot detect the chip. I connected usb dongle to see if my keyfob is the
problem. The debugger could not detect usb dongle as well. The key fob works fine as well as dongle. I checked with BT stack.
I followed every step in FAQ in instruction documents but still no luck. Is this faulty debugger?
I do not know whether it works before I update firmware. I was told to update the firmware first in flash programmer.
If this is faulty programmer, where can I request to replace? I purchased it with overnight shipping and it turns out to be defective device.