Hi:
In cc2640 SDG 5.1.4,There is a description as below:
"Due to controller processing limitations in the stack, additional rules exist (beyond what the specification
defines) that must be followed when multiple simultaneous connections exist. These rules are as follows.
• All intervals of the connection must be multiples of each other. If not, the connection does not form or
the parameters do not update."
I have 3 slaves,which connection interval is correct for device1,device 2 and devic 3?
A)500ms,500ms,500ms
B)500ms,1000ms,1500ms
C)500ms 1000ms,2000ms
Best regards
Dan