Hi
Am working on off chip oad which is working fine I can able to download the new image using the downloader and can able to store the image in external flash.
And after downloading bim will check the meta data and load the corresponding new image on to the internal flash
My question is on handling error cases like if large image or crc mismatch happen in between when bim loading firmware on to the external flash
Is there any ble profile in order to notify these errors like crc mismatch,large image, same image while doing OAD off chip? ??
I want to identify these type of errors and notify these errors to the mobile using profile or any type of notification in the application side? ??
How this type of errors are handled in oad process???
Please suggest any way or answer will be appreciated
Thanks in advance! !!!!