Other Parts Discussed in Thread: CC2640, CC2650
Hi,
I need help to save values in memory flash.
I read the datasheet development but i don't understand how to save values in flash memory.
I code this :
//*******OSAL_SNV************//
uint8 Item_id = 0x80; //This is in bcomdef.h
uint8 snv_status;
/*Save*/
snv_status = osal_snv_write(BLE_NVID_THOMAS,sizeof(value), value);
/**Control save**/
if ( snv_status == 0) //Sauvegarde Ok
SensorTag_blinkLed(Board_LED2, 5);//G
else //Sauvegarde PAS OK
SensorTag_blinkLed(Board_LED1, snv_status);//R
//***************************//
But my LED1 blink two like snv-status, thus it return "OSAL_SNV Value = 2" if we understand the "3.10.4 Using Simple NV" in the datasheet development. I tryed to erase memory with
"osal_snv_iinit(void)" but it doesn't work.
Thanks,