Im a electrical engineering student, now I still doing my final project for the graduation. My final project in about CC2541 and when I write program, there are some errors like this.
Error[e16]: Segment XDATA_I (size: 0xd72 align: 0) is too long for segment definition. At least 0x565 more bytes needed. The problem occurred while processing the segment placement command "-Z(XDATA)XDATA_Z,XDATA_I=_XDATA0_START-_XDATA0_END", where at the moment of placement the available memory
ranges were "XDATA:16f3-1eff"
Reserved ranges relevant to this placement:
XDATA:1-eff XSTACK
XDATA:f00-1eff XDATA_Z
BIT:0-7 BREG
BIT:a8-af SFR_AN
BIT:e8-ef SFR_AN
Whats is the solution of this problem? or maybe for the long time I write program in RAM memory CC2541? and how to move my program from uint buffer to Flash memory in CC2541? Thanks