This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650 ADC minimum sampling rate to sample signal of certain frequency

Other Parts Discussed in Thread: CC2650

Hello,

I am a bit confused about the minimum sampling rate required to correctly sample signal of certain frequency in CC2650 ADC. In Sensor Controller Studio, I fixed the sampling rate at 2kHz by calling function:

adcStartAuxTimer0Trigger(500);

And I tried periodic sine waves of different frequencies: 100Hz, 200Hz, 500Hz, and 1kHz.

It seems ADC with sampling rate fixed at 2kHz is only able to correctly sample sine waves of 100Hz. So the ratio of ADC sampling frequency/signal frequency is 2kHz/100Hz=20. Here shows the figures:

This is sine wave of 100Hz.

This is sine wave of 500Hz:

I am a bit surprised that the ratio is 20. Normally 12-bit ADC takes 14-cycle data conversion and 10-cycle hold time, so according to Nyquist theorem, the minimum ratio should be (10+14)*2=48? Did I make any mistakes here?

Your feedback will be greatly appreciated! Thanks!

Best,

Xiaoxiao