This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: Android, OTA Upgrade and CE

Genius 5355 points
Other Parts Discussed in Thread: CC2541

Hi Support,

Customer is evaluating CC2541DK-SENSOR.

#1. During the process of writing/reading characteristic to/from CC2541 with Android devices (version 4.4), the transmission speed is very slow.It is significantly slow comparing to iPhone mobile devices. Searched through the forum and it seems like other users also encounter this issue but it has not been resolved.

#2. Need to implement firmware upgrade. Is there any reference coding of over-the-air for both IOS and Android OS?

#3. For CE testing, is there any information available so that we can minimize some testing cost?

Thanks.