This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just a quick question (and possibly a stupid one) but in the data sheet for the MPU 9250 (as on the SensorTag), it says that the reset value to write to the PWR_MGMT_1 register is 0x01
However in the SensorTag firmware source code, the reset value written is 0x80 (which is exactly the reverse of the 0x01).
Say for example I am writing into the PWR_MGMT_1 register, and I want bit [7] to be 1 and [6:0] to be 0 - do I have to write basically the reverse of what I am thinking?