Other Parts Discussed in Thread: CC2564
Hi
I am trying assisted mode A2DP (A3DP) and it looks like all vendor commands are executed successfully and the sequence too seems to be as per the requirement but when a song is played from remote device the SBC packets are still routed to host stack rather then decoded on the BT controller
Can some one tell if they have come across this issue and how to resolve this.
Strangely one is 20-25 attempts the packet are played at controller but it is all noise and it is very discontinuous.
seq is : AVPR enable sink mode during stack init. After receiving a2dp connect indication issue 1) open sink stream on a2dp 2) configure PCM and A3DP codec settings on a2dp start indication 3) call start sink stream
Thanks
regards
Nitin